Hi,
I would like to seek some recommendations on the best TI components to use in my power supply design with a customer.
Design 1:
Input Requirements: 18-36V
Output Requirements: 27V 7.4A and above (200W)
Isolation Requirements: Best scenario is that the Input and Output are isolated, but if not, nonisolated is ok.
Design 2:
Input Requirements: 18-24V
Output Requirements: 27V 11A and above (300W)
Isolation Requirements: Best scenario is that the Input and Output are isolated, but if not, nonisolated is ok.
Thanks,
Shuanglin