Good morning,
I want to use the UCC28710 in a Flyback application with an input voltage range of 12V - 36V DC.
I am confident it will work but would like to have your consent.
I am asking because Webench does not allow me to input this voltage range.
I will not be using the HV pin of the UCC28710 and will leave it floating.
I want to use the UCC28710 because of its constant voltage constant current capability.
Thank you.