Other Parts Discussed in Thread: LM5145, , PMP7282, PMP20178, LM5146
Hi,
Requirement of DC-DC Buck Converter
Vin = 48Vdc
Vout min = 5Vdc
Vout max = 40Vdc
Iout min = 0.5A
Iout max = 30A
I wanted to design programmable DC-DC buck converter using LM5116/LM5145 whose output voltage changes by changing the feedback pin voltage using DAC.
All the design calculation in datasheet of LM5116/ LM5145 are considering fixed output voltage.
The webench design can not be used for wide range output voltage (such as 5VDC to 40VDC).
Please guide how to design the programmable DC-DC buck converter using LM5116/LM5145 for above listed requirement
Also I have checked the reference design http://www.ti.com/tool/PMP7282