Other Parts Discussed in Thread: LM3643, LM3644
I want to power 4 lasers in series using TPS61165. The lasers characteristics is like a LED, but we need continuous current here. For each laser, the maximum current is 170mA, and the forward voltage of laser is 1.6V-1.7V. I want to know whether the output current is continuous or not? Can I reduce the output current ripple by increasing the value of the output capacitance if the current is continuous? And is it possible to reduce the current ripple into 1mA?