Other Parts Discussed in Thread: LP8758
Hi,
In data sheet P.46 "inductor selection", it is stated that the effective inductance value should be 0.33 μH or more.
What is concerned when using an inductor smaller than 0.33 μH?
Best regards,
Yuto Sakai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yuto,
Thanks a lot for your interest in our PMIC device! The major concern is the stability of the loop control provided by LP8758 inside design; also, DC output performance, like ripple, etc. will be impacted.
Please let's know if you have more questions.
Thanks!
Phil
Hi, Yuto-san,
A1: Yes, adding external capacitance can help the loop stability.
A2: No, we don't have the data of phase margin and gain margin; all data about the loop stability has been shown in datasheet in time domain as transient response.
FYI, all parameters in datasheet are simulated, tested and validated based one 0.47uH (+/-30%) inductance value.
Please let's know if you have more questions.
Thanks!
Phil
Hi Phil-san,
Thank you for your reply.
For A1, is the added capacitor an output capacitor (Cout)? Or feed-forward capacitors?
If it is feed-forward capacitor, How shoud it be connected?
Also, when the effective inductance value is less than 0.33 μH, how much extra external capacitor should be added?
Best regards,
Yuto Sakai