This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65311-Q1: Shutdown sequence using SPI LPM0 and PWR_CONFIG resgister?

Part Number: TPS65311-Q1

While i am in active state am i able to use the PWR_CONFIG register to disable power supplies in a determined sequence and than transition into LPM0 mode so buck 1 is turned off last?

  • Hi Julio,

    Reading through the datasheet, it looks like writing the BUCKx_EN bits to 0 should disable the bucks and they can determine that sequence by the SPI write order, though it will be immediate. Then LPM0 can be entered and they will have already been disabled.

    I've looped in our expert in case there is more to it than that.