I want to use the TPS26000 but I don't need the shutdown feature. What is the best practice with regards to the SHDN pin? Leave it open? Connect it directly or via a resistor to the input? The nominal input voltage is 15 volts in my case, so connecting the pin to the input would be way off its recomennded operating conditions.