This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24210: BQ24210 not charging lipo battery

Part Number: BQ24210


I've built the following circuit based on the BQ24210 IC in order to charge a lipo battery from USB (~5VDC) or a solar panel. I'm first trying to make the circuit work from VBUS (USB) = 5VDC, what is actually injecting 4.75VDC on the VBUS pin.

EN_SOLAR (EN pin) is pulled low all the time by the MCU. VBUS_RDY is also read by the MCU and it stays at 0V when both the USB cable and the battery are connected  to the board. However CHG always stays high (D6 OFF), which means that the charger is not charging the battery. I then thought that R8 (R_VDPM) was maybe too low so I removed the resistor for battery tracking mode but the problem persists. The circuit seems to never charge the battery.

Thanks in advance for your help.