This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2844 as Gate Driver

Other Parts Discussed in Thread: UC2844

Please check the attached document.

We use UC2844 as Gate Driver.

We want to fix the frequency(50kHz) and Duty(25%).

We think that This IC can fix the duty cycle if we connect VFB pin and VREF pin. Because voltage of Vref is 5V fixed.

So It is not affected by voltage fluctuation.

Please tell us the value of R1 and R2 when Duty is 25%.

Best regards,

Takahiro Nishizawa

Question of UC2844.pdf