Dear sir,
I want to charge android phone using the battery of an Auto Rickshaw which is usually of 12 volts. Is there any reference design available ?
Regards,
Manoj Hiwarkar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sir,
I want to charge android phone using the battery of an Auto Rickshaw which is usually of 12 volts. Is there any reference design available ?
Regards,
Manoj Hiwarkar
Yes, correct I want to use 12V Auto Rickshaw Battery as the input source to charge the phone. OK if charger IC is already designed inside the phone isn't there any protection circuitry required? can I feed 12v directly to the phone? if no then please suggest me a proper regulator ic for that.