Other Parts Discussed in Thread: BQ51003
The datasheet of the BQ51013B is a bit confusing regarding the operating temperature. The maximum junction temperature starts at -40 and 125°C and all Electrical Characteristics are specified at this temperature range, but still the "Recommended operating temperature" starts at 0°C.
Can somebody from TI explain why the recommended operating temperature starts at 0°C, and can I get a confirmation if the device can actually be used below 0°C?