Other Parts Discussed in Thread: LM5166
Hi,
I am going to use TPS54062 for a low power step down conversion. Input voltage range is from 36V to 52V. There is a limitation on input current of 5mA. i.e. input current shall not exceed 5mA. Required Output is 12V/ 10 mA.
Now for this, application, is TPS54062 suitable? TPS54062 needs external bootstrap capacitor to turn on high side N channel MOSFET. During each PWM cycle, this capacitor will charge from input supply and input current will exceed 5mA for certain amount of time right? Can you please suggest solution to this problem?
Is adding a series resistor to bootstrap capacitor a good solution? This will limit the switching frequency and duty cycle.