Hello,
I am using the lm5140 in a design with the default 3.3V and 5V outputs for Vo1 and Vo2. When the FB pins are tied to VDDA as shown in the reference schematic, What is the ideal ripple injection point for testing the control loop response?
I am using a sense resistor on the output, so my thought was to place a 20ohm resistor between on the sense line back to VOUT1 but this seems does not seem like the correct way to test. Is it required to use a resistor divider on the feedback pin and use a standard ripple injection resistor instead of tieing the pin to VDDA?
Thanks