This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23625: The LMR23625 heats up.

Part Number: LMR23625


Hi,

I use the LMR23625CQDDARQ1 in a typical application.

The layout is according to recommendations in DS.

Input voltage = 24V.

Output voltage = 5V

Output current = 300mA.

The DC/DC, L15 and C163 heat up to 55 degrees Celsius.

Please suggest solution!