This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27531: Can I make "ground of UCC27531 negative and shift the IN and EN signals accordingly?

Part Number: UCC27531


Team: Can I make "ground of UCC27531 negative and shift the IN and EN signals accordingly?
For example:
GND=-10V, VDD= 5V,
IN and EN=-10V to -7V
Output= -10V to  5V

Thanks.