Other Parts Discussed in Thread: BQ25120A, BQ25121A
Hello.
I'd like to measure the current consumption of the IC to verify the number suggested by datasheet.
I am powering the EVM with SMU 5V with no load on DC/DC converter output.
With Vsys 1.8V it consumes 1.66mA(without charging, load) but if I set Vsys 2.5V it consumes 2.6mA.
So far there's some current consumption through LED, resistors etc. but it seems that internally there's something that I cannot see via datasheet of EVM.
Is there any method to measure the current consumption of bq25120a on idle state with EVM?
Regards,
Hyobin