Other Parts Discussed in Thread: BQ34Z100, BQ34Z100EVM, EV2400, BQSTUDIO
Hello,
I have several questions regarding the BQ34Z100-G1 evaluation module, more specifically on integrating the calbration/golden image on higher scale volumes.
- Is it recommended to determine the battery pack characteristics characteristics on the BQ34Z100EVM or with the product using the BQ34Z100 itself?
- Once the calibration, learning cycle etc is done with the EV2400 on a single product, can this golden image accurately be used on all other products and programmed with a STM32? In other words, is calibration required on each of the products or will once suffice?
- Due to mechanical constraints we cannot apply a temperature sensor directly to the pack in the final product (for safety however, other measurements are done). Is it possible to only use the temperature sensor during the qualification process to create the golden image and use that golden image and the chip internal temperature sensor onwards?
Thanks!