Other Parts Discussed in Thread: FUSION-PRODUCTION-GUI, UCD3028, UCD3020
Hi all,
May i know the differences between Production tool vs Manufacture tool? what issues does Production tool fix than Manufacture tool?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
May i know the differences between Production tool vs Manufacture tool? what issues does Production tool fix than Manufacture tool?
I am verifiying the difference and get back to you.
Regards,
Hi all,
May i know the differences between Production tool vs Manufacture tool?
No difference right? Only software update reason?
what issues does Production tool fix than Manufacture tool?
I didn't get answers,could you list on document for me? thank you for help.
Production tool departed from Manufacturing tool long time ago.
There are many builds of Production tool that aim to address many enhancements and fixes:
Build 1.2.126 [December 16, 2015]
Build 1.2.127 [January 4, 2016]
Build 1.2.128 [April 21, 2016]
Build 1.2.129 [April 25, 2016]
Build 1.2.130 - Build 1.2.131 [April 27,2016]
Build 1.2.32 [May 4, 2016]
Build 1.2.133 [May 9, 2016]
Build 1.2.134 [May 17, 2016]
Build 1.7.000 [July 5, 2016]
Build 1.7.001 [August 4, 2016]
Build 1.7.002 [August 5, 2016]
Build 1.7.003 [August 8, 2016]
Build 2.0.0 – 2.0.3 [August 25, 2016 – Sept 21, 2016]
Build 2.0.4 [September 26, 2016] (Not released)
Build 2.0.5 [September 28, 2016]
Build 2.0.6 [October 4, 2016]
Build 2.0.7 [February 22, 2016]
Build 2.0.8 [June 30, 2017]
Build 2.0.9 [July 31, 2017]
-----------------------------------------------------------------------
Here are some examples:
Build 1.2.126 [December 16, 2015]
Bug Fixes
* When clicking export of script – exception dialog would appear about NI assembly references.
Build 1.2.127 [January 4, 2016]
Updates
I’ve added support for reading a serial number consisting of letters and numbers.
There is also support for downloading to two devices on different SAA adapters with one of the them having the control pin 5 pulled low.
Build 1.2.129 [April 25, 2016]
Updates:
* Remove need for implementing commands 0xE4 and 0xE5 (cmds_dcdc_paged and cmds_dcdc_nonpaged). Useful for firmware not implementing pmbus commands
. If they do not have E4/E5 it will not complain and if they do it will work. I will also be making a fusion studio gui that will have device GUI respond the same way as you had mentioned before as they didn’t like when the error shows up during the scan and we recommended setting the bitmask to zero. Now if they don’t have the bitmask for the device GUI it will not show an error however if they use the online gui they will not see many configuration commands as that is based on the bitmask.
----------------------------------------------------------------
If you have used the Manufacturing tool and it works for you. Stay with that one.
If you have anew use case, start with Production tool.
The expert with these tools will be back after Labor day and will help you with specific requests that you might have.
I'M INTERESTING IN THIS SENTENCE"There is also support for downloading to two devices on different SAA adapters with one of the them having the control pin 5 pulled low. ",IT MEANS CAN I USE PRODUCTION TOOL DOWNLOAD FIRMWARE TO 2 DEVICES WITH 2 USB-TO-GPIO AT SAME TIME?
COULD YOU GIVE US SUGGESTIONS & DOCUMENT FOR THIS ?THANKS.
Yes, that is exactly what this means.
This feature exists only in Production tool and is supported in Build 1.1.127 from January 2016 and up.
The operation is quite easy, pin #5 which is the control pin on on one of the interfaces needs to be pilled low (Zero logic).
This way the software can distinguish between the two interfaces. Please give it a try and let us know if you have any other questions.