Other Parts Discussed in Thread: LM5122, LM5170
Hi, All:
Customer want to use TPS43060 for applicate condition --> Vin = 12V, Vout = 54V Iout = 10A
Could you help to check the applicate condition is ok or not?
Other, I used webench that show some information as below.
===========================================
With the current design condition, suitable FET components M1 and M2 could not be found in the current database. Hence, this design is created using ideal FETs. Please note that the resulting FET parameters are ideal, so the efficiency and loss values (related to FET) have been disabled. Also, schematic/PCB export and thermal simulations will not work with ideal FET.
===========================================
It mean customer can used TPS43060 if they can find a MOSFET same as webench used, right?