This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS565201: Minimum output capacitor for 0.9V output application

Part Number: TPS565201


Dear expert,

We would like to design a 10~12Vin to 0.9Vout@3.5A solution with TPS565201.

In datasheet, the minimum output cap is 22uF. I think it is the same with 0.9Vout application.

But in webench designer, it will recommend 55uF.

Can I design this application with "22uF +feed forward cap(4.7pF)"? 

Ben