Other Parts Discussed in Thread: TPS65920, OMAP3530
There is not information about the purpose of this input signal on the TPS65920/30/50? Should it be tied high or low and what is the function?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Howard Robson said:There is not information about the purpose of this input signal on the TPS65920/30/50? Should it be tied high or low and what is the function?
There is an application note entitled TPS65950 and OMAP3530 Hardware Connectivity User's Guide (Rev. A) which provides an illustration of the proposed connection in Figure 2.
In addition, there is a schematic checklist on the TPS65950 Product Folder which should be helpful.
Thank you, I had not noticed that this document was available. It is a big help in verifying that I have got all the connections between the OMAP3530 and the TPS65920 correct.
Hi
Do you have Schematic checklist for OMAP3530, used while reviewing the schematic for new design.
Which document provides info for UNUSED pins, what need to be done for OMAP 3530. We are not using few interfaces, what need to be done for such unused pins.
Warm Regards
Prabhu
Hi,
You may want to ask this on the OMAP forum. I do not have the information you need for OMAP.
Regards,
Gandhar.
Hi,
Enclosed OMAP Design Review checklist....