I have a question about the operation of the BQ24040 ISET2 pin.
My Setup:
ISET resistor = 2.2k (~250mA target charge current)
My Observed operation:
ISET2 = 0: charge current = ~250mA
ISET2 = float: charge current = ~100mA
ISET2 = high: charge current = ~250mA
From the datasheet, it appears that when ISET2 is floating or high, it operates independently of the ISET resistor. My observations would indicate that when ISET2 is high, the charge current is the lower of the ISET value or 500mA. Can you confirm that my observations match the expected operation of the device?