Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
I have imported the TPS54239 model to TINA from Webbench. While attempting for Transient analysis in TINA, the simulation runs successfully if I select "Calculate Operating point" whereas when I select "Zero initial conditions" or "Use Initial conditions" the results are not as expected. I take care of following during the simulation: -
Go to Analysis >> Options and enable the following options
a) dis-able warning for large size analysis
b) percentage bar
c) Enable instant diagram drawing
Go to analysis >> Set analysis parameters . Click on hand symbol and choose default
Go to analysis >> Transient. Ensure that "Draw extraction" is un-checked
As "Calculate operating point" takes more time, I prefer to perform simulation with "Zero initial conditions"
Can you please help to resolve?
Thanks - Babu