Other Parts Discussed in Thread: TPS2376HEVM, , , TPS2372
I designed a PoE PD board using the TPS2375PWR-1 device. When providing a PoE source the output power cycles, as shown in the attached scope trace.
I have the TPS2376HEVM eval board and when I connect the same PoE source it works fine, so I don't think there is a problem with the source (even though the eval boards uses a slightly different version of the PD chip). The design is based on the example in the datasheet and I tried modifying some values but I always get basically the same result. The power comes on for about 0.5s, and then goes off again, repeating every ~3s.