Other Parts Discussed in Thread: BQ24725A, BQSTUDIO, EV2400
Hi, team!
I use the BQ28Z610 in the control board of the 2S Li-ON battery(mini-UPS) and the chip is in a sealed state. I do not have neither EVM or i2c BQ programmer - only my microcontroller (atmega328 with the Arduino bootloader).
When I reading the data block for the unseal key(0x0035), the data is returned from the previous successful MAC read (e.g. OperationStatus 0x0054) and it means that I can not read the unseal key in sealed mode.
I successfully read from standard registers and MACdata, but I can not normally configure the chip because it is sealed. I learned this forum on similar topics of unlocking BQs and I find out that I need default unseal keys for transferring the chip to unseal mode. I saw in some topics that many who encountered this problem were recieve a key by email.
Can you also send me a default unseal key?
My email: niskorodnov@lanit.ru
As I understand it is necessary to write a unseal key (4 bytes) to the register 3E with the command 0x0035 with a checksum, or another procedure? I write the program in the Arduino IDE environment on a C ++ similar language using the standard Wire library.
For MACdata block read, I do this:
- Open connection with BQ i2c address and send 0x3E(allManAcces) and command bytes(LSB, MSB) - first transaction with closing connection.
- Open connection with BQ i2c address and send 0x3E(allManAcces) and read MAC block(36 bytes) - second transaction with closing connection.
What transfer procedure should be used to transfer the chip from SEALED to UNSEALED mode and UNSEALED to FULL ACCESS?
Unfortunately, the manual(SLUUA65B) does not very clearly explain what specific operations you need to perform, and there is nowhere in the datasheets an understandable structure for data transmission (for example, for the BQ24725A that I use in the project - there the query structure is shown superbly). I read it across and in the part of the security modes, but still the procedure is incomprehensible for transferring to UNSEALED mode, there is only an example for replacing the keys, which only works if the chip works in unseal mode.
PS: Why do we need such big difficulties with unlocking the device and all these keys? Why not specify a default keys in datasheet/tech guide?