The TPS61194 datasheet states: "TPS61194 detects LED output configuration during start-up. Any current sink output connected to ground is disabled and excluded from the adaptive voltage control of the DC-DC and fault detections."
Can this connection to ground be made with a pull-down resistor instead of a direct connection? We would like the same HW design to support backlights with both 3 and 4 strings.
We've considered using a FET to short the 4th output to ground in 3 string cases, but don't want to have the potential for a ground short in the 4 string case present in the design.