Part Number: TPS61071
Other Parts Discussed in Thread: TPS61070
Tool/software: WEBENCH® Design Tools
Hello,
I want to use the TPS61070 as a step-up converter to 5.5V from one cell Li ion batterie.
But when i want to measure the FB Voltage, VOut is breaking down to 2.3V and afterwards the TPS61070 has a permanet damage.
In the first place is the TPS61070 the wright boost converter for my application because i want 5.5 and at least 70mA Output current.
In the Webbench they recommend 3.6V as maximum Vin.
And do i damage the IC when i want to measure between FB an ground?
I hope you can help me Thanks in advance.
Alex