Part Number: LM3434
Dear all,
could you please advise on the best replacement for LM3434, which is now obsolete? It needs to drive currents up to 36Amps.
Some specs:
Operating Input Voltage : 12VDC – 24VDC
Buck topology CCM
I (led) max : 32Amp
Analog LED current adjust - Tie to an external reference to adjust the average LED current
En – Enable pin
DIM – Digital Input for dimming the LED (control the DIM FET (shunt))
Soft start
Longevity > 6 years
Thanks,
Federico Papparotto