Other Parts Discussed in Thread: ASH,
TLV62569 Used as 5V to 3.3V ,When the load at 420ma ,the ripple of 3.3V is very high(140mVpp)then test SW pin ,SW PIN show is switch at PWM and PFM mode ,the ash as below ,When i set L16 2.2uH to 1uH,The ripple down to 270mA,the swing of work mode came to better , What is the reason ? If there any hidden trouble?
picture1 is sch , picture2 is ripple high . picture 3 is normal mode ,