This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23630: Min Cboot

Part Number: LMR23630


Hi

I have a related question about this thread.

I understood there are no any data for min Cboot. However our customer need to estimate how much variation of Cboot can be acceptable.

How much is the variation of Cboot can be acceptable? +/-50%? or +/-100%?

Best Regards,

Koji Hamamoto

  • Koji,

    We definitely do not recommend -100%

    The datasheet suggests Cboot of 100nF or 470nF. This means selecting a 470nF will allow your variation to drop to ~20% of the rated value before you even reach the other recommended value of 100nF. This is the conservative route if that's what they're looking for.

    -Sam