This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65051 working with imx25 reset circuit



Dear  

 
We are using your TPS65051 in an own design following all your documentation. We have a doubt related to document SLVA403, "Powering the Freescale™ i.MX25 Using the TPS65051".  
 
The problem is with RESET circuit. In page 6 of the application note, using the corresponding calculations and values of resistors you provided (R5=237k, R6=3.01k, R15=180k), VH=2,3V and VL=2,26V which is not a possible value if voltage to these resistors is VLDO4 (in that case 1.6V).  
 
We are not sure if these calculations are incorrect or we are missunderstanding something.