This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5008: QUESTION ABOUT TI's PRODUCT

Part Number: LM5008
Other Parts Discussed in Thread: CSD19532Q5B

hello,

i am using TI's LM5008 IC with my solar panels to convert high DC voltage into 5V. LM5008 is rated for 100v as per datasheet.

my solar panel is giving MAX. 105 V at the start up ( open circuit voltage) and when my load is connected (after 100ms) it drop down at 70-75 volts.

so my question is, can LM5008  survive at that moment when my solar panel system having 105V  for 100ms. ?????

also same thing is happening with TI's SMD MOSFET CSD19532Q5B????

So please answer for both components.

thank you.