Other Parts Discussed in Thread: UCC27712, , , UCC27712EVM-287, UCC27212
Hello team,
Hope you are doing well. Please see below question from the customer:
I prototyped using the UC27714. For proof of concept, I used 2 of the UCC27712 evm boards and stacked them in this same configuration and got sine wave at the outputs which are the switch nodes of the evm boards (On my prototype board, they are TP1 and TP2). I noticed that the evm board has 4 bulk capacitors on the HV rail and my board does not have any cap on the HV rail. My bench power supply is pretty hefty one and I am sure it has lots of bulk capacitance at the output. Some of the E2E forum discussed about switching too fast could prevent the boot capacitor not to have time for charging. But, that does not seem to be the case here, because it works with he evm boards. Please advise
Input = 400V DC @ 2A
Output = As high as possible 500 - 600W (Goal is to output DC Sine wave 20 kHz)