This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659037: TPS65903x

Part Number: TPS659037

If the Cin and Cload ( capacitive load driving capability)vlaues are not available , what reasonable values can be assumed?

I need to know the Cin and Cload values for each pin of TPS65903x( where ever applicable)

  • Bhargav,

    Hi, thanks for reaching out to us on E2E.

    The recommended capacitor values for the TPS659037 can be found in the spec table of the datasheet, with descriptions in section 6.2.2: www.ti.com/.../tps659037.pdf

    In summary,
    LDOx_IN pins: 2.2uF typical
    LDOx_OUT pins: 2.2uF typical
    SMPSx_IN pins: 4.7uF typical
    SMPSx_OUT pins: 47uF typical
    VBG pin: 0.1 uF typical
    VCC1 pin: 10uF typical
    OSC decoupling caps: 10pF (per side of the crystal)

    Please let me know if this is what you are looking for.

    Thanks,
    Nastasha