I don’t see the TPS62235 in SwitcherPro. Even though it’s 2MHz instead of 3MHz, could I use the same reference design as the TPS62232?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I don’t see the TPS62235 in SwitcherPro. Even though it’s 2MHz instead of 3MHz, could I use the same reference design as the TPS62232?
Thanks!
Per the datasheet, you should use a 1 or 2.2uH inductor and a 4.7uF output capacitor. So, yes, the same as the model for the 62232.