This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24166: Impedance in the charging path

Guru 11170 points
Part Number: BQ24166


Hello E2E,

Our customer builded the trial production board using bq24166.
That board has charge cut off circuit. When battery voltage to be lowest, that circuit to be active. It's for safety charging operation.

Cut off circuit has the following configuration.
 [bq24166] - [P-FET *2] - [10uF *2] - [CMC] - [Battery]

P-FET has 0.1-ohm on-resistance.
CMC has 1uH inductance.

Normally charging current is 1-A.

Question.
When switched the charging mode CC to CV, Is bq 24166 affected by the charging path?

Regards,
ACGUY