We have a constant power load, and hence have selected Load Mode = 1 (Section 6.2 of Tech Ref manual). We also wish to use the 'Reserve Capacity' feature. From Section 6.2 (relevant passage copied below)
Given we have Load Mode =1, we entered the reserved capacity in the 'Reseve Cap-cWh' section if the IT Cfg data memory. However, this did not seem to do anything; remaining capacity is unaffected by changing this value. However, changing the value in 'Reserve Cap-mWh' does change remaining capacity as expected, regardless of load mode. This seems to be incorrect behaviour.
The log file linked below shows that 'Reserve Cap-mWh' causes a change to remaining capacity (after a reset) regardless of Load Mode, and 'Reseve Cap-cWh' has no impact in either load mode.
/cfs-file/__key/communityserver-discussions-components-files/196/3566.res_5F00_cap.log
Please can you advise if this is a bug, known issue, or if there are other settings that must also be applied to use 'Reseve Cap-cWh'