This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: Max battery capacity

Part Number: BQ27510-G3
Other Parts Discussed in Thread: BQ27510

Hi

What is the true max battery capacity for this part. There appears to be different answers depending upon where you look.

When viewed in the parametric list of fuel gauge products on the website, the max battery capacity is shown as 16Ah.

In the datasheet the value given is 32Ah in section 1: Features.

Then in the firmware change document from version G2 - G3 (slua686.pdf) it is given as 14.5Ah using the Des Energy Scale feature.

Which is the correct figure? Have a 20Ah battery and I'm trying to work out if the device is suitable for such an application.

Many Thanks

Andy