This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About materials with fly-buck

Part Number: LM5160


HI,

Could you tell me about the material of fly-buck configuration using LM5160?

【Q1】
For the following application notes,do you measure the efficiency in a circuit without photo coupler (Figure 2)?



【Q2】
For the following EVM User's Guide,why is the upper limit of Vin 32V?



Best regards,
Yuto Sakai

  • Yuto-san,

    1. We did not measure the efficiency of the non-opto solution. The efficiency should be improved by not having the opto but it may be reduced by the 1.6k minimum load on the secondary output.

    2. This board was designed to work for nominal 24V battery input which typically ranges from 18V to 32V. It was optimized to work best at these voltages but the board could be operated at higher voltages since the IC is a 65V part and the input caps are rated to 100V.

    -Sam