Need to find a Component at lowest possible cost that can drive external MOSFETs so that the
stepup can deliver 24V 8A. This will not be done on a continous basis but now and then. The 12V will
be on all the time and the 24V must be there, but the full 8A output will only be drawn during a couple of seconds and then it will rest for at
a minute or two Before next high current output is needed.
Any suggestion? TPS43060?