I am fairly new to pcb deisgn.I wanted to understand isolation for power supplies for the board I am designing. The board would have a couple of ADCs, DACs and microcontroller. It would be powered with a 24V supply which needs to stepped down to 15V,5V and 3.3V. The topology that I have is 24 to 15V isolated and the 15V to 5V and 3.3V non isolated. The 15V, 5V and 3.3V rails are for ADCs, DACs and Serializers. Should I have another 24V to 3.3V isolated power supply for the microcontroller and CAN transceiver? Or can I do another non isolated 15V to 3.3V? Any help would be useful. Thanks!
Harini