This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54201: How about the input impedance/current of PWM pin of TPS54201?

Part Number: TPS54201

Hi team,

As you know the PWM input of TPS54201 is multifunction, it is used for PWM/analog dim input, and also for PWM/analog dim mode configuration. To keep the device operate in PWM mode the amplitude of PWM signal should be within 1.0V to 2.07V. However the PWM signal from controller is 0V to 5V. To meet the requirement of TPS54201 the 0V/5V pwm signal has to be divided down. However TPS54201 datasheet does not specify the input impedance of PWM pin which is must to design the value of divider. Could anyone provide the spec?

Thank you,

John