Other Parts Discussed in Thread: UCC27212A-Q1
Hi Team,
Customer is looking for auto HB gate driver which is capable of Vin_min=7.5V, system operating voltage.
LM5109B-Q1 is good for candidate, but recommended operating range is 8V to 14V, but I think max UVLO is 7.4 in spec, so UVLO does not hit when the system is operating at Vin=7.5V.
But I would like to know if VDD is less than 8V but over 7.4V, the device works or any de-rating? Regards, ny