Hello,
I currently have 3 packs returned that have 20-30 ohms measured between VCC and GND. This circuit is setup similar to the circuit in the reference design, with a diode and 1uF capacitor. The only difference is that we have an added 10 ohm resistor inline to create an RC filter with the capacitor. On all 3 of these units, we found the 10 ohm was open, which is an indication that this was drawing too much current. Sure enough, we are getting the short circuit on VCC.
What can cause this failure?
Thanks,
Mike