My design requires the battery to be located 6 inches away from the main board. The link between the battery and the main board, will be awg22 wires with 2 connectors. Therefore the impedance between the battery and the main board will probably vary depending on wires, contacts, etc.
My questions:
Is the BQ27500 affected by different system impedance between itself and the battery?
Is it OK to put the BQ on the main board, or should I put it on a small PCB close to the battery? (doing so means my cable has 8 conductors instead of 6).