Hi team,
My customer want to use the LM4040AxxI in -40degree to 105degree.
But they need to make sure maximum Average temperature coefficient is 100 ppm/C
For the LM4040Axxl, the recommendation temp is -40 to 85.
1. So can you help to provide when the temperature is up to 105 degree, what specs will be degrade and how worse.
2. What's the maximum Average temperature coefficient when the temperature is between the -40 and 105 degree?
Thanks a lot!
Lacey