Hi,
I am basically a firmware engineer but trying to get into hardware design as well now, so I have a basic question on power section.
In my scenario, I have a controller which would require 1A current and a GPRS module which would need 2A at times.
While designing the power section what are the considerations I must follow? Please give me some points to start off.
Suppose some DC-DC converter says that maximum current to be given at input of IC is 2A but if I connect say a adapter with current rating of 3A, what would be the result?
Thanks,
Janardan M