Other Parts Discussed in Thread: CSD87355Q5D
I see the inbuilt current and temperature sensor, But I dont see much information on how to use them? Is there a gain factor that relates current senses to analog Voltage output? Does Vref has to be 5/2 v ? Also, is the current output ( voltage) calibrated to the temperature? Does that use the same temp that is output for temp sensor output. What's the accuracy and linearity of the inbuilt sensor outputs?
Also, what is the Rdson and Qg(tot) of the MOSFETs? Are the two mosfets exactly the same?
How to calculate efficiency if current and pwm freq is known
Id like to use it as a half bridge , ie use 3 of these to make a hex bridge to drive a 3 phase brushless PMDC motor. is that possible? It looks like a IC solution instead of 2 mosfets, 1 dual gate drivers IC, 1 current sensor IC and 1 temperature sensor IC. So, its great for formfactor.