Tool/software: WEBENCH® Design Tools
Good afternoon.
I drew an scheme with bq25606.
Made a circuit board(4 layers). I tried to do everything according to the description.
In the end: I give to the input 5V (the battery did not connect), at the output I have this picture:
why is the signal waveform (saw) on the output? So it should be?
I connect the load 5 ohms, I give to the input 5V. The output voltage is 1.76V. I raise the voltage to 7.2V, the output voltage stabilizes (saw like without load). Where is the mistake?
If the load is fed to the stabilizer already included, then the voltage remains normal (saw at 3.6V).
FB1 is NM.