This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27621-G1: Please suggest for proper solutions for single cell

Part Number: BQ27621-G1
Other Parts Discussed in Thread: BQ2980, BQ2970, , BQ27742-G1

Hi, 

My customer is searching for the solutions for single cell Li-lon battery, 

Spec: 

Battery: 8300mAh 3.8V

Can you help to confirm if this part is a proper solution? 

Please let me know if further information needed. 

thank you.

  • Hi,

    For the protector,
    My first suggestion is BQ2980, please also help to double check if this part is the proper for the single protector.
    Thanks for your help.
  • Hi!
    The bq2980 is a the most accurate and high-featured single-cell protector. For a simpler protector they can look at the bq2970 family. They will need to select the correct part number to match the protection thresholds they require.
    bq27621-G1 can also work for their gauge, but there are many other options. bq27742-G1 is an example which integrates the protection and gauge function in one IC.